AXIS#.IL.COMPTABLE.ENABLE
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.COMPTABLE.ENABLE returns the current output of the cogging compensation/torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist compensation table.
See AXIS#.IL.COMPTABLE.DATA for more information how the table operates.
Example
Once a cogging map/torque map has been loaded, it can be turned on for Axis 1 by setting to 1:
-->AXIS1.IL.COMPTABLE.ENABLE 1
To disable a cogging map/torque map that has been loaded, set the same keyword to 0:
-->AXIS1.IL.COMPTABLE.ENABLE 0
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-03-000 |
General Information
|
Type |
Read//Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.COMPTABLE.ENABLE | 0x500A | 0x19 | UINT | 1:1 | - | RW | False |
| AXIS2.IL.COMPTABLE.ENABLE | 0x510A | 0x19 | UINT | 1:1 | - | RW | False |